Fire departments rely on MiniTec's modular system for equipping buildings and workshops as well as upgrading vehicles. The range for breathing protection workshops has now been revised.
MiniTec draws on its decades of experience in the development and manufacture of ergonomic workstation systems for industry and production when designing respiratory protection workshops. This expertise benefits the individual needs of respirator attendants. Individual work steps such as dismantling, cleaning, testing, assembly and documentation are brought into an ideal flow with standardized workstation modules in the respiratory protection workshop and adapted to the available room dimensions. The program for fire departments is constantly being developed further, including the modular system for respiratory protection workshops.
The new work surface is ideal for the black area.
The material 1.4301 with a very fine grind K400 is now used for the stainless steel worktops. This is ideal for the black area, where cleaning and disinfecting the surface is a top priority. Individual worktops up to a length of four meters can be freely configured with a wide variety of sinks, draining surfaces, anti-splash edges, drip edges and many other elements and thus adapted to the customer-specific situation.
Ergonomic shower sets are also new: the long hose, which is guided in a long metal spiral, allows you to reach every corner with the water-saving shower head. The swivel spout can be conveniently operated with the elbow, preventing contamination through contact transfer.
The shower set can be used flexibly.
The new drawers are simply practical.
The new generation of drawers is characterized by a high level of comfort and durability. The telescopic runners - with very smooth retraction - have a load capacity of 70 kg. Thanks to the carefully selected materials, the drawers are water-resistant and therefore ideal for damp rooms.
The front elements made of highly durable HPL plastic are now available in light gray and anthracite as standard.
Shelves are now available in two versions. With stainless steel and melamine-coated chipboard, it is now possible to adapt the interior of the furniture to the conditions in the room.
There are also new options for doors and shelves.
Would you like to find out more about MiniTec solutions for fire departments? You can find all the important information here!