Autumn and winter are a popular time for model building enthusiasts to construct new aircraft and ships or to revise existing models. It is not uncommon for a kitchen table or door leaf to be converted into a base for the tedious and highly precise work.
It is obvious that this is not ideal for objects whose value quickly reaches the 5-digit range. You often have to stretch or remain in a strenuous posture for a long time in order to perform certain activities. If you want to work on different parts of a model at the same time, there is often not enough space. Many model builders therefore want a professional work table that meets their special requirements in terms of functionality and ergonomics.
The team from "Die Modellwerker" in Gersheim, Saarland, knows these needs from their own experience and has therefore designed a versatile work table that is ideally suited to the requirements of model building. Central elements are a particularly torsion-resistant tabletop and the MiniTec aluminum profile construction kit.
On this basis, a flexible solution with numerous advantages was created:
A video presentation provides practical information about all the features and advantages of the work table.
Of course, the table not only makes sense for model making, but can also be used for a wide variety of assembly work. For example, when it comes to manually assembling or processing small and medium-sized series of any product. Or to flexibly carry out joining or soldering operations or to assemble cable harnesses. The range of applications is huge.