The Helmholtz-Zentrum Berlin for Materials and Energy works closely with MiniTec . There, among other things, clean rooms were built and equipped with a profile construction for the construction of a particle-free ultra-high vacuum chamber with which semiconductor photocathodes can be transferred to an SRF photoinjector. The Institute Silicon Photovoltaics operates two clean rooms for performing silicon-based semiconductor technology processes. The setups there are constantly changing, which requires flexibility in the design elements.
The MiniTec modular system is also in use for the BESSY II project, which is concerned with materials for a sustainable energy supply and the operation of an electron storage ring.
The large number of projects and the very different applications show how flexible MiniTec's modular system is. And the philosophy true to the company slogan "The Art of Simplicity" is also a good basis in this area.