Low space requirement, maximum flexibility!
MiniTec has added a highly interesting product to its range in the area of conveyor systems: The new mini conveyor belt is characterized by a very small space requirement and is used to transport small parts.
The core component is a special 45 mm aluminum profile (Profile 45 FRS), which can be seamlessly integrated into any MiniTec construction. It acts as a base and carrier profile for a 25 mm wide conveyor belt. The length of the conveyor belt can be between 250 mm and 2000 mm.
Either a head drive or a center drive is used as the drive, i.e. it can be placed either at the end of the conveyor section or within it. The head drive is equipped with a servo motor, for the center drive either a three-phase AC motor or a servo motor can be taken. Which motor is the most suitable depends on the situation and the requirements. If the speed is to be variable, servo motors are recommended, because with these the speed can be changed continuously. With three-phase motors, on the other hand, the speed is fixed and is either 3.4 or 4.3 or 6.6 m/min, depending on the type. However, the speed can also be variably adjusted here by means of a frequency converter (accessory).
Wide range of applications
The range of applications for the new mini conveyor belt is huge. Wherever small parts have to be transported, the solution can be integrated quickly and easily - due to its simple design, of course, also by the customer himself. And because the 45 FRS profile serves as the basis, mini conveyor belts can also be used for feeding or discharging materials in combination with MiniTec's FRS kanban system.
Premiere at LogiMAT 2022
The mini conveyor belt will be presented to the public for the first time at LogiMAT from May 31 to June 2, 2022. Visitors can take a look at the extremely practical solution at MiniTec in Hall 1 at Stand L08 and see its flexibility and advantages for themselves live.