New holders for workstation systemEasy attachment of parcel tape hand rollers and thin client computers 29. July 2024

An ergonomically optimized working environment ensures higher performance, efficiency and processing quality. This is why MiniTec workstation systems have extensive options for ergonomic adjustment. Two new options have now been added in the area of holders.

Holder for parcel tape hand roller

At many workstations, products or workpieces have to be packaged, often using hand-held packaging tape dispensers. MiniTec now has a practical holder to ensure that these are always to hand. It can be fitted to the profile system in just a few simple steps and ensures more order and efficiency at the workplace.

Article no. 32.0085/0 | Details and ordering

Holder for thin client computers

A clear trend in the workplace can be seen in the area of digitalization. Whether it's the MiniTec SmartAssist assistance system or another application, the need to attach appropriate computer hardware is usually a direct consequence. This is why MiniTec now also offers a holder for thin client computers, which can be easily attached to MiniTec monitor supports.

Article no. 32.0612/1 | Details and ordering

 

The adhesive tape roller holder is used to store hand-held tape dispensers at the workplace. Space-saving and conveniently mounted on the profile, it ensures tidiness and cleanliness.

The Thin Client holder can be easily attached to the MiniTec monitor support.