MiniTec presents solutions for material flow and warehouse management as well as battery production at the digital trade fair platform LogiMAT.digital.
At the end of May 2022, MiniTec will present innovative solutions for intralogistics, materials handling and materials management at the Logimat trade fair in Stuttgart. Already in advance, interested parties can inform themselves about innovations on the virtual platform Logimat.digital. On April 6, 2022, from 10 to 11 a.m., MiniTec will present the advantages of an integrated solution in the lecture "Intelligent warehouse logistics with integrated materials handling technology." Participation is free of charge: https://logimat.digital
Proper warehouse logistics avoid costly mistakes
Among other things, the focus is on a warehouse logistics system. This supports the optimization of materials and warehouse management and thus makes a decisive contribution to minimizing costs and ensuring the competitiveness of a company. Key benefits include time and space savings, personnel savings, error minimization, better information management and the automated handling of items. The manufacturer has been using the warehouse logistics system with fast and space-saving warehouse lifts, conveyor lines from its own range and a connection to the existing ERP landscape for several years itself and has been able to optimize its processes significantly as a result.
Precision and speed in battery production
Assembly systems for battery production are another focus of the exhibition. Here, both precision (the tolerances are within narrow limits) and speed (the cells have to be glued and welded together in a short time) are important criteria. Accordingly, the transport of the module bodies or pack housings requires a technology that ensures high process and repeat accuracy. Conveyor systems from the manufacturer are used here, which transport workpiece carriers with high precision and speed.
Handling systems based on linear axes, which are characterized by precision and a flexible design, are used for pick-and-place of the battery modules with the individual cells. This also applies to the operations of gluing and pressing the battery cells in the module. In the automation of handling areas by MiniTec, robots can also be integrated.
Article from https://www.digital-manufacturing-magazin.de/logimat-so-etablieren-sie-eine-intelligente-lagerlogistik/